NXOpen.UF.Draw.AskRevolvedSxline¶
-
Draw.
AskRevolvedSxline
()¶ Refer to UF_DRAW_ask_revolved_sxline for documentation.
Signature:
AskRevolvedSxline(sxlineTag)
Parameters: sxlineTag (Tag) – Tag of revolved section line to query Returns: A Tuple Return type: A tuple consisting of (stepDir,arrowDir,pviewTag,rotptObject,numSxviews,sxviewTags,numSxsegs,numLeg1Sxsegs,cutPlaneLeg,sxsegTags,sxlineStatus) stepDir(list of float): Step direction vector (unitized) relative to the drawing: step_dir[0] = x value step_dir[1] = y value step_dir[2] = z value
arrowDir(list of float): Arrow direction vector (unitized) relative to the drawing: arrow_dir[0] = x value arrow_dir[1] = y value arrow_dir[2] = z value
pviewTag(Tag): Parent view tag
rotptObject(
`NXOpen.UF.Drf.Object
Refer to UF_DRF_object_s for documentation.`): Object associated to rotation pointnumSxviews(int): Number of section views associated to section line
sxviewTags(list of Tag): Array of section line’s section view tags Use UF_free to free memory
numSxsegs(int): Number of section line segments.
numLeg1Sxsegs(int): Number of section segments input to define the first leg. Cannot be greater than num_sxsegs. Any remaining segments define leg2.
cutPlaneLeg(
`NXOpen.UF.Draw.SxlineLeg
Refer to UF_DRAW_sxline_leg_e for documentation.`): Leg used to define cut plane = UF_DRAW_sxline_leg1 = UF_DRAW_sxline_leg2sxsegTags(list of Tag): Array of section line segment tags Use UF_free to free memory
sxlineStatus(
`NXOpen.UF.Draw.SxlineStatus
Refer to UF_DRAW_sxline_status_e for documentation.`): Section line statusLicense requirements: None