NXOpen.UF.Draw.AskHalfSxline¶
-
Draw.
AskHalfSxline
()¶ Refer to UF_DRAW_ask_half_sxline for documentation.
Signature:
AskHalfSxline(sxlineTag)
Parameters: sxlineTag (Tag) – Tag of half section line to query Returns: A Tuple Return type: A tuple consisting of (stepDir,arrowDir,pviewTag,numSxviews,sxviewTags,numSxsegs,sxsegTags,sxlineStatus) stepDir(list of float): Step direction vector (unitized) relative to the drawing: step_dir[0] = x value step_dir[1] = y value step_dir[2] = z value
arrowDir(list of float): Arrow direction vector (unitized) relative to the drawing: arrow_dir[0] = x value arrow_dir[1] = y value arrow_dir[2] = z value
pviewTag(Tag): Parent view tag
numSxviews(int): Number of section views associated to the input section line
sxviewTags(list of Tag): Array of Section line’s section views Use UF_free to free memory
numSxsegs(int): Number of section line segments
sxsegTags(list of Tag): Array of section line segment tags Use UF_free to free memory
sxlineStatus(
`NXOpen.UF.Draw.SxlineStatus
Refer to UF_DRAW_sxline_status_e for documentation.`): Section line statusLicense requirements: None