NXOpen.UF.DispSrfanlData_Struct.ScaleFactor¶
-
DispSrfanlData_Struct.
ScaleFactor
¶ scale factor applied to the data range The range of the scalar function in all ‘face analysis’ faces in the NX part is called the ‘data-range’. Some portion of this range is mapped to displayed colors (from red through green to blue). This mapped range is centered at ‘mid_value’ and has size equal to the size of the data_range times the ‘scale_factor’. The ‘mid_value’ and ‘scale_factor’ are directly controllable by the NX user, using sliders on the ‘face analysis’ dialog. This is only for GAUSSIAN type