NXOpen.UF.DispSrfanlData_Struct.ReflMovePosition¶
-
DispSrfanlData_Struct.
ReflMovePosition
¶ reflection translation or rotation factor. This is used when the reflection movement type has been set. Must be a value between UF_DISP_REFL_TRANSLATE_MIN and UF_DISP_REFL_TRANSLATE_MAX when refl_move_type is set to translate or between UF_DISP_REFL_ROTATE_ANGLE_MIN and UF_DISP_REFL_ROTATE_ANGLE_MAX when refl_move_type is set to rotate.