NXOpen.UF.DispSrfanlData_Struct.AnalFacetWidthTol¶
-
DispSrfanlData_Struct.
AnalFacetWidthTol
¶ Facet width tolerance for analysis display. This value is ignored unless the surf_anal_fineness member is set to UF_DISP_SHADED_CUSTOMIZE_TOL. This value specifies the maximum width of a facet. The recommended value is .3. A smaller tolerance value causes a finer display but also causes slower performance. A value of .075 would give a fine display, .02 an extra fine display, and .005 an ultra fine display. @@ Refer to the SAMPLE=uf_disp_tab1.html tolerance mapping table ENDSAMPLE @@