NXOpen.UF.DispSrfanlData_Struct.AnalFacetEdgeTol¶
-
DispSrfanlData_Struct.
AnalFacetEdgeTol
¶ This is the facet edge tolerance for shaded display. This value is ignored unless the surf_anal_fineness member is set to UF_DISP_SHADED_CUSTOMIZE_TOL. This is an upper bound on the distance from each chord to the curve it is approximating The recommend value is .005 inch.Smaller values result in finer display but causes degraded performance. A value of .01 would give a coarse display, .0005 would give an extra fine display but also causes slower performance. @@ Refer to the SAMPLE=uf_disp_tab1.html tolerance mapping table ENDSAMPLE @@