NXOpen.UF.DispSrfanlData_Struct.AnalFacetChordTol¶
-
DispSrfanlData_Struct.
AnalFacetChordTol
¶ This is the facet chord distance for shaded display. This value is ignored unless the surf_anal_fineness member is set to UF_DISP_SHADED_CUSTOMIZE_TOL. This is an upper bound on the distance from a positions on a facet to the surface. The recommended value is .005 inch. A smaller value results in a finer display but causes degraded performance. A value of .01 would give a coarse display, .0025 would give a fine display, .001 an extra fine display and .0005 an ultra fine display. @@ Refer to the SAMPLE=uf_disp_tab1.html tolerance mapping table ENDSAMPLE @@