NXOpen.UF.DispSrfanlData_Struct.AnalFacetAngleTol¶
-
DispSrfanlData_Struct.
AnalFacetAngleTol
¶ This is the facet angle tolerance for shaded display. This value is ignored unless the surf_anal_fineness member is set to UF_DISP_SHADED_CUSTOMIZE_TOL. This is an upper bound on the angular deviation between the surface normals at any two positions under the facet. The recommended value is 15 degrees. A smaller value results in a finer display, but causes slower performance. A coarse display would use a tolerance of 0.0, 15.0 gives the standard angle, a value of 6.0 would give an extra fine display, and a value of 3.0 an ultra fine display. @@ Refer to the SAMPLE=uf_disp_tab1.html tolerance mapping table ENDSAMPLE @@