NXOpen.UF.Disp.Inquire Structure¶
NXOpen.UF.Disp.Inquire is an alias for NXOpen.UF.DispInquire_Struct
-
class
NXOpen.UF.
DispInquire_Struct
¶ Bases:
object
Refer to UF_DISP_inquire_s for documentation.
Fields
NXOpen.UF.DispInquire_Struct.ContextRunning |
Describes the context which is being executed when the inquire is performed. |
NXOpen.UF.DispInquire_Struct.IsViewModeValid |
True if the view mode was returned and False if no information was available |
NXOpen.UF.DispInquire_Struct.ViewMode |
View mode describes the views shading and face analysis mode valid values are UF_VIEW_NOT_SHADED UF_VIEW_PARTIALLY_SHADED UF_VIEW_FULLY_SHADED UF_VIEW_ANALYSIS_SHADED See uf_view.h for definitions |
NXOpen.UF.DispInquire_Struct.IsAttenPtValid |
True if the atten point was returned and False if no information was available |
NXOpen.UF.DispInquire_Struct.AttenPt |
The attention point of the geometry just displayed |
NXOpen.UF.DispInquire_Struct.IsDrawOpenDisp |
Is the drawing view open for display? If true then geometry may be added to the drawing. |
NXOpen.UF.DispInquire_Struct.ViewTag |
View tag of the view being displayed |