NXOpen.UF.Cutlevels.Single StructureΒΆ
NXOpen.UF.Cutlevels.Single is an alias for NXOpen.UF.CutLevelsSingle_Struct
Fields
NXOpen.UF.CutLevelsSingle_Struct.EntityTag |
Tag id of the face or point entity used to define the current cut level. |
NXOpen.UF.CutLevelsSingle_Struct.ZLevel |
The z distance of the cut level from the origin along the normal of the cut levels. |
NXOpen.UF.CutLevelsSingle_Struct.LocalCutDepth |
The max depth per cut value to be used for the range between this cut level and the one above it. |