NXOpen.UF.CutLevels.Load¶
-
CutLevels.
Load
()¶ Refer to UF_CUT_LEVELS_load for documentation.
Signature:
Load(operationTag)
Parameters: operationTag (Tag) – The tag of the operation for which thecut levels are defined. Returns: A new data structure containing all of the cut levels for the specified operation. The pointer to the structure must be NULL on input, or it must be a valid pointer created using a previous call to UF_CUT_LEVELS_load. The pointer must be freed by UF_CUT_LEVELS_free. Return type: list of NXOpen.UF.CutLevels.CutLevels
Refer to UF_CUT_LEVELS_s for documentation.License requirements: None