NXOpen.UF.CutLevels.EditLevelUsingZ¶
-
CutLevels.
EditLevelUsingZ
()¶ Refer to UF_CUT_LEVELS_edit_level_using_z for documentation.
Signature:
EditLevelUsingZ(operationTag, editLevel, zLevel, maxDepthPerCut)
Parameters: - operationTag (Tag) – The tag of the operation for which thecut levels are defined.
- editLevel (int) – The index of the level to be edited(0 being the top level).
- zLevel (float) – The z distance, along the tool axis,of the cut level from the origin.
- maxDepthPerCut (float) – The max depth per cut to be used forsubdividing the range above the new cut level.
Returns: If the data structure created bya call to UF_CUT_LEVELS_load is passed in, then it will be updated to reflect the changes from the addition. If NULL is passed in, then the argument is ignored.
Return type: NXOpen.UF.CutLevels.CutLevels
Refer to UF_CUT_LEVELS_s for documentation.License requirements: None