NXOpen.UF.CutLevels.EditLevelUsingGeom¶
-
CutLevels.
EditLevelUsingGeom
()¶ Refer to UF_CUT_LEVELS_edit_level_using_geom for documentation.
Signature:
EditLevelUsingGeom(operationTag, editLevel, geomTag, maxDepthPerCut)
Parameters: - operationTag (Tag) – The tag of the operation for which thecut levels are defined.
- editLevel (int) – The index of the level to be edited(0 being the top level).
- geomTag (Tag) – The tag of the face or point definingthe new cut level.
- maxDepthPerCut (float) – The max depth per cut to be used forsubdividing the range above the new cut level.
Returns: If the data structure created bya call to UF_CUT_LEVELS_load is passed in, then it will be updated to reflect the changes from the addition. If NULL is passed in, then the argument is ignored.
Return type: NXOpen.UF.CutLevels.CutLevels
Refer to UF_CUT_LEVELS_s for documentation.License requirements: None