NXOpen.UF.CutLevels.DeleteLevel¶
-
CutLevels.
DeleteLevel
()¶ Refer to UF_CUT_LEVELS_delete_level for documentation.
Signature:
DeleteLevel(operationTag, deleteLevel)
Parameters: - operationTag (Tag) – The tag of the operation for which thecut levels are defined.
- deleteLevel (int) – The index of the cut level to bedeleted (0 being the top level).
Returns: If the data structure created bya call to UF_CUT_LEVELS_load is passed in, then it will be updated to reflect the changes from the deletion. If NULL is passed in, then the argument is ignored.
Return type: NXOpen.UF.CutLevels.CutLevels
Refer to UF_CUT_LEVELS_s for documentation.License requirements: None