NXOpen.UF.CutLevels.AskTopOffLevel¶
-
CutLevels.
AskTopOffLevel
()¶ Refer to UF_CUT_LEVELS_ask_top_off_level for documentation.
Signature:
AskTopOffLevel(cutLevels, index)
Parameters: - cutLevels (
NXOpen.UF.CutLevels.CutLevels
Refer to UF_CUT_LEVELS_s for documentation.) – The loaded cut levels data structure. - index (int) – The index of the top off level the datais required for (0 being the top level).
Returns: Address of the pointer to the data ofthe requested single level. The address must not be NULL on input. The data includes: - The tag of the face or point entity used to define the current cut level. This can be NULL if the level was defined by an explicit z level. - The z distance of the cut level down from the top cut level. All values will be non-negative. - The max depth per cut value to be used for the range between this cut level and the one above it.
Return type: list of
NXOpen.UF.CutLevels.Single
Refer to UF_CUT_LEVEL_single_s for documentation.License requirements: None
- cutLevels (