NXOpen.UF.CutLevels.AddLevelsUsingZ¶
-
CutLevels.
AddLevelsUsingZ
()¶ Refer to UF_CUT_LEVELS_add_levels_using_z for documentation.
Signature:
AddLevelsUsingZ(operationTag, numToAdd, zLevels, maxDepthPerCut)
Parameters: - operationTag (Tag) – The tag of the operation for which thecut levels are defined.
- numToAdd (int) – The number of z-levels being added.Value must be non negative.
- zLevels (list of float) – Array of z distances, along the tool axis, of the cut level from the origin.
- maxDepthPerCut (float) – The max depth per cut to be used forsubdividing the range above the new cut levels. A value of zero indicates that there is no limit. Value must be non negative.
Returns: If the data structure created bya call to UF_CUT_LEVELS_load is passed in, then it will be updated to reflect the changes from the addition. If NULL is passed in, then the argument is ignored.
Return type: NXOpen.UF.CutLevels.CutLevels
Refer to UF_CUT_LEVELS_s for documentation.License requirements: None