NXOpen.UF.Curve.PtSlopeCrvatr Structure¶
NXOpen.UF.Curve.PtSlopeCrvatr is an alias for NXOpen.UF.CurvePtSlopeCrvatr_Struct
-
class
NXOpen.UF.
CurvePtSlopeCrvatr_Struct
¶ Bases:
object
Refer to UF_CURVE_pt_slope_crvatr_s for documentation.
Fields
NXOpen.UF.CurvePtSlopeCrvatr_Struct.Point |
3D coordinates of input ordered points. For creating periodic curves, you should not repeat the first point as the last point |
NXOpen.UF.CurvePtSlopeCrvatr_Struct.SlopeType |
type of control being defined: UF_CURVE_SLOPE_NONE, UF_CURVE_SLOPE_AUTO, UF_CURVE_SLOPE_VEC, UF_CURVE_SLOPE_DIR (see Note 1) |
NXOpen.UF.CurvePtSlopeCrvatr_Struct.Slope |
3D vector defining the slope assigned at this input point (see Note 1, 4, 5) |
NXOpen.UF.CurvePtSlopeCrvatr_Struct.CrvatrType |
type of control being defined UF_CURVE_CRVATR_NONE, UF_CURVE_CRVATR_AUTO_DIR, UF_CURVE_CRVATR_VEC (see Note 2) |
NXOpen.UF.CurvePtSlopeCrvatr_Struct.Crvatr |
3D vector defining the curvature assigned at this input point (see Note 2, 3, 6) |