NXOpen.UF.Curve.OcfValues Structure¶
NXOpen.UF.Curve.OcfValues is an alias for NXOpen.UF.CurveOcfValues_Struct
-
class
NXOpen.UF.
CurveOcfValues_Struct
¶ Bases:
object
Refer to UF_CURVE_ocf_values_s for documentation.
Fields
NXOpen.UF.CurveOcfValues_Struct.String |
A character string used to hold an offset value in form of a string (e.g “2.0”) to offset the string on the input set of faces. |