NXOpen.UF.Curve.IntersectInfo Structure¶
NXOpen.UF.Curve.IntersectInfo is an alias for NXOpen.UF.CurveIntersectInfo_Struct
-
class
NXOpen.UF.
CurveIntersectInfo_Struct
¶ Bases:
object
Refer to UF_CURVE_intersect_info_s for documentation.
Fields
NXOpen.UF.CurveIntersectInfo_Struct.TypeOfIntersection |
type of intersection found = 0 -> none = 1 -> 3D intersection = 2 -> 2D intersect ion |
NXOpen.UF.CurveIntersectInfo_Struct.CurvePoint |
intersection point coordinates on curve |
NXOpen.UF.CurveIntersectInfo_Struct.CurveParm |
parameter value of intersection point on curve |
NXOpen.UF.CurveIntersectInfo_Struct.EntityParms |
parameter value(s) of intersection point on entity, both values are valid when the entity is a body or face, neither value is valid for a plane or datum plane, otherwise only the first value is used |