NXOpen.UF.Curve.BridgeData Structure¶
NXOpen.UF.Curve.BridgeData is an alias for NXOpen.UF.CurveBridgeData_Struct
-
class
NXOpen.UF.
CurveBridgeData_Struct
¶ Bases:
object
Refer to UF_CURVE_bridge_data_s for documentation.
Fields
NXOpen.UF.CurveBridgeData_Struct.Method |
creation method |
NXOpen.UF.CurveBridgeData_Struct.InputCurve1 |
First input string, must contain only one curve or edge. |
NXOpen.UF.CurveBridgeData_Struct.InputCurve2 |
Second input string, must contain only one curve or edge. |
NXOpen.UF.CurveBridgeData_Struct.MatchptParms |
Location parameter on input strings, used as a percentage along the string, must be an expression or a number between 0.0 and 100.0 |
NXOpen.UF.CurveBridgeData_Struct.MatchPoint |
Location reference points (optional) |
NXOpen.UF.CurveBridgeData_Struct.ReverseTangents |
True= Reverse Tangents, False = Dont Reverse Tangents |
NXOpen.UF.CurveBridgeData_Struct.ShapeControl1 |
Shape ControlFor UF_CURVE_match_*_ends: Tangent magnitude at first input curve, must be an expression or a number greater than 0.0. |
NXOpen.UF.CurveBridgeData_Struct.ShapeControl2 |
Shape ControlFor UF_CURVE_match_*_ends: Tangent magnatude at second input curve, must be an expression or a number greater than 0.0 For UF_CURVE_match_*_peak: Controls skew at peak point, must be an expression or a number between 0.0 and 100.0 |
NXOpen.UF.CurveBridgeData_Struct.StiffnessMethod |
Controls (to some extent) the degree, continuity, and complexity of the curve 0 = automatic 1 = low 2 = high |
NXOpen.UF.CurveBridgeData_Struct.InheritCurve |
Reference shape string, must contain only one curve or edge. |