NXOpen.UF.Curve.SectionFromRadialPlanes¶
-
Curve.
SectionFromRadialPlanes
()¶ Refer to UF_CURVE_section_from_radial_planes for documentation.
Signature:
SectionFromRadialPlanes(generalData, radialData)
Parameters: - generalData (
NXOpen.UF.Curve.SectionGeneralData
Refer to UF_CURVE_section_general_data_s for documentation.) – Data providedby the user to to be used in creating the section curve feature. - radialData (
NXOpen.UF.Curve.SectionRadialData
Refer to UF_CURVE_section_radial_data_s for documentation.) – Data provided bythe user describing the radial planes.
Returns: Feature tag, if general_data->associate is 1, or Group tag of section curves if general_data->associate is 0 and general_data->grouping is 0, or Group tag of groups of curves if general_data->associate is 0 and general_data->grouping is 1
Return type: License requirements: SOLIDS MODELING or DRAFTING
- generalData (