NXOpen.UF.Curve.SectionFromParallelPlanes¶
-
Curve.
SectionFromParallelPlanes
()¶ Refer to UF_CURVE_section_from_parallel_planes for documentation.
Signature:
SectionFromParallelPlanes(generalData, parallelData)
Parameters: - generalData (
NXOpen.UF.Curve.SectionGeneralData
Refer to UF_CURVE_section_general_data_s for documentation.) – Data providedby the user to to be used in creating the section curve feature. - parallelData (
NXOpen.UF.Curve.SectionParallelData
Refer to UF_CURVE_section_parallel_data_s for documentation.) – Data providedby the user describing the parallel planes.
Returns: Feature tag, if general_data->associate is 1, or Group tag of section curves if general_data->associate is 0 and general_data->grouping is 0, or Group tag of groups of curves if general_data->associate is 0 and general_data->grouping is 1
Return type: License requirements: SOLIDS MODELING or DRAFTING
- generalData (