NXOpen.UF.Curve.EditTrimCurve¶
-
Curve.
EditTrimCurve
()¶ Refer to UF_CURVE_edit_trim_curve for documentation.
Signature:
EditTrimCurve(curveTag, boundingId, refPoint, intPoint, extInd)
Parameters: - curveTag (Tag) – tag of curve to trim
- boundingId (Tag) – tag of first bounding object ( curve, edge, plane, face, point)
- refPoint (list of float) – ref_point[3] are the coordinates of a point used to specify which portion of the curve to trim also used as start point intersection point iteration (ACS)
- intPoint (list of float) – int_point[3] is the start point for finding the intersection of the curve to trim and the bounding object.
- extInd (int) – shape of the extension of the curve: UF_CURVE_NATURAL_SHAPE UF_CURVE_LINEAR_SHAPE UF_CURVE_CIRCULAR_SHAPE
License requirements: SOLIDS MODELING or DRAFTING