NXOpen.UF.Curve.EditJoinedFeature¶
-
Curve.
EditJoinedFeature
()¶ Refer to UF_CURVE_edit_joined_feature for documentation.
Signature:
EditJoinedFeature(joinedCurveFeature, ufCurveString, creationMethod, tols)
Parameters: - joinedCurveFeature (Tag) – CRV_JOIN feature
- ufCurveString (
NXOpen.UF.Modl.StringList
Refer to string_list for documentation.) – string of input curves. Use UF_MODL_init_string_list and UF_MODL_create_string_list to create input strings. Use UF_MODL_free_string_list to free memory after the string is created. - creationMethod (int) – 1 - Polynomial Cubic, 2 - General Spline 3 - polynomial quintic 4 - Advanced
- tols (list of float) – Tolerances [0] - distance tol [1] - angle tol [2] - string tol
License requirements: SOLIDS MODELING or DRAFTING