NXOpen.UF.Curve.CreateLinePointPrincipalAxis¶
-
Curve.
CreateLinePointPrincipalAxis
()¶ Refer to UF_CURVE_create_line_point_principal_axis for documentation.
Signature:
CreateLinePointPrincipalAxis(point, principalAxis, limitP, supportPlane, isAsso)
Parameters: - point (Tag) – tag of start point
- principalAxis (
NXOpen.UF.Curve.PrincipalAxis
Refer to UF_CURVE_principal_axis_e for documentation.) – one of the 3 principal axes : UF_CURVE_X_AXIS, UF_CURVE_Y_AXIS, UF_CURVE_Z_AXIS - limitP (list of
NXOpen.UF.Curve.Limit
Refer to UF_CURVE_limit_s for documentation.) – extension limits - supportPlane (Tag) – tag of support plane of the line
- isAsso (bool) – true - if associative, false - if not associative
Returns: if is_asso == TRUE - object identifier of new associative line feature if is_asso == FALSE - object identifier of new associative line
Return type: License requirements: SOLIDS MODELING or DRAFTING