NXOpen.UF.Curve.CreateLinePointPoint¶
-
Curve.
CreateLinePointPoint
()¶ Refer to UF_CURVE_create_line_point_point for documentation.
Signature:
CreateLinePointPoint(point1, point2, limitP, supportPlane, isAsso)
Parameters: - point1 (Tag) – tag of start point
- point2 (Tag) – tag of end point
- limitP (list of
NXOpen.UF.Curve.Limit
Refer to UF_CURVE_limit_s for documentation.) – extension limits - supportPlane (Tag) – tag of support plane of the line
- isAsso (bool) – true - if associative, false - if not associative
Returns: if is_asso == TRUE - object identifier of new associative line feature if is_asso == FALSE - object identifier of new associative line
Return type: License requirements: SOLIDS MODELING or DRAFTING