NXOpen.UF.Curve.CreateJoinedFeature¶
-
Curve.
CreateJoinedFeature
()¶ Refer to UF_CURVE_create_joined_feature for documentation.
Signature:
CreateJoinedFeature(ufCurveString, creationMethod)
Parameters: - ufCurveString (
NXOpen.UF.Modl.StringList
Refer to string_list for documentation.) – string of input curves. Use UF_MODL_init_string_list and UF_MODL_create_string_list to create input strings. Use UF_MODL_free_string_list to free memory after the string is created. - creationMethod (int) – 1 - Polynomial Cubic,2 - General Spline 3 = polynomial quintic 4 = advanced
Returns: A Tuple
Return type: A tuple consisting of (joinedCurveFeature,status)
joinedCurveFeature(Tag): CRV_JOIN feature
status(int): 0 = Curve has no corners1 = Curve has corners
License requirements: SOLIDS MODELING or DRAFTING
- ufCurveString (