NXOpen.UF.Curve.CreateBridgeCurve¶
-
Curve.
CreateBridgeCurve
()¶ Refer to UF_CURVE_create_bridge_curve for documentation.
Signature:
CreateBridgeCurve(bridgeMethod, curveIds, parms, reverseTangent)
Parameters: - bridgeMethod (int) – UF_CURVE_TANGENT - match tangents UF_CURVE_CURVATURE - match curvatures
- curveIds (list of Tag) – Object identifiers of the two curves/edges to bridge.
- parms (list of float) – Parameters on curves/edges to connect bridge.
- reverseTangent (list of int) – Indicates whether to reverse the tangent direction vector at the chosen parameter on the curve/edge. 0 = do not reverse not 0 means to reverse
Returns: Object identifier of the bridge curve.
Return type: License requirements: SOLIDS MODELING or DRAFTING