NXOpen.UF.Curve.AskWrapParms¶
-
Curve.
AskWrapParms
()¶ Refer to UF_CURVE_ask_wrap_parms for documentation.
Signature:
AskWrapParms(wrapCurveObject)
Parameters: wrapCurveObject (Tag) – Object Identifier of the wrap or unwrap feature. Returns: Pointer to a structure to be filled in with the defining information for the input feature. The calling routine must allocate a UF_CURVE_wrap_data_t structure, and pass the pointer into this routine. This routine will fill the structure with allocated data. The calling routine must then call UF_CURVE_free_wrap_parms to free memory allocated to support this structure. Return type: NXOpen.UF.Curve.WrapData
Refer to UF_CURVE_wrap_data_s for documentation.License requirements: None