NXOpen.UF.Curve.AskCurveInflections¶
-
Curve.
AskCurveInflections
()¶ Refer to UF_CURVE_ask_curve_inflections for documentation.
Signature:
AskCurveInflections(curveEid, projMatrx, range)
Parameters: - curveEid (Tag) – Object identifier of the curve
- projMatrx (list of float) – Projection matrix specified in a 1D arra y(proj_matrx[9])
- range (list of float) – Lower and upper limit of the relative range (in %) in which inflection points are searched range[0] = lower limit (umin) range[1] = upper limit (umax)
Returns: A Tuple
Return type: A tuple consisting of (numInfpts,infPts)
numInfpts(int): Number of inflection points found
infPts(list of float): The inflection points data. The size of the array is inf_pts[num_infpts * 4]. (*inf_pts+4*i)[0] = u value of the ith inflection. [1-3]= x, y, z values of the ith inflections. This array must be freed by calling UF_free.
License requirements: None