NXOpen.UF.Curve.AskArcLength¶
-
Curve.
AskArcLength
()¶ Refer to UF_CURVE_ask_arc_length for documentation.
Signature:
AskArcLength(curveTag, startParam, endParam, unitFlag)
Parameters: - curveTag (Tag) – Tag of curve to query for arc length
- startParam (float) – Start parameter of the curve from which the arc length is to be calculated. (Normalized parameter)
- endParam (float) – End parameter of the curve to which the arc length is to be calculated. (Normalized parameter)
- unitFlag (
NXOpen.UF.Modl.Units
Refer to UF_MODL_units_e for documentation.) – Any one of the following enumerated constants: UF_MODL_UNITS_PART - same as parts units UF_MODL_INCH - inches UF_MODL_MMETER - millimeters UF_MODL_CMETER - centimeters UF_MODL_METER - meters
Returns: arc length of the curve from start_param to end_param.
Return type: float
License requirements: None