NXOpen.UF.Csys.MapPoint¶
-
Csys.
MapPoint
()¶ Refer to UF_CSYS_map_point for documentation.
Signature:
MapPoint(inputCsys, inputPoint, outputCsys)
Parameters: - inputCsys (int) – CSYS of point to be mapped which can be: UF_CSYS_ROOT_COORDS ( Coordinate space of the root part which is the whole part being displayed), UF_CSYS_WORK_COORDS ( Coordinate space of the work part), UF_CSYS_ROOT_WCS_COORDS ( Root WCS)
- inputPoint (list of float) – The point (xyz) to be mapped.
- outputCsys (int) – CSYS to be mapped to
Returns: The resultant point (xyz) of the mapping
Return type: list of float
License requirements: None