NXOpen.UF.Clone.LogFileFailure Structure¶
NXOpen.UF.Clone.LogFileFailure is an alias for NXOpen.UF.CloneLogFileFailure_Struct
-
class
NXOpen.UF.
CloneLogFileFailure_Struct
¶ Bases:
object
Refer to UF_CLONE_log_file_failure_s for documentation.
Fields
NXOpen.UF.CloneLogFileFailure_Struct.LineNumber |
line number in the log file on which the error was detected |
NXOpen.UF.CloneLogFileFailure_Struct.InputPartName |
with UF_free part name being processed when error occurred, may be NULL |
NXOpen.UF.CloneLogFileFailure_Struct.InvalidToken |
with UF_free token which was invalid, may be NULL |