NXOpen.UF.Clone.GenLogOpts Structure¶
NXOpen.UF.Clone.GenLogOpts is an alias for NXOpen.UF.CloneGenLogOpts_Struct
-
class
NXOpen.UF.
CloneGenLogOpts_Struct
¶ Bases:
object
Refer to UF_CLONE_gen_log_opts_s for documentation.
Fields
NXOpen.UF.CloneGenLogOpts_Struct.DefaultAction |
enum value indicating the default action to be applied to components |
NXOpen.UF.CloneGenLogOpts_Struct.DefaultNaming |
enum value indicating the default naming technique to be applied to components |
NXOpen.UF.CloneGenLogOpts_Struct.CopyNonmasterOpts |
a linked list of nonmaster_type/logical pairs indicating whether those nonmaster types should be copied during the clone, import or export operation. Only relevant in a NX Manager environment, may be null. |
NXOpen.UF.CloneGenLogOpts_Struct.DefaultValidationOpts |
a data structure indicating the options to control whether and how the validation objects should be created during the import operation. Only relevant for import operation in a NX Manager environment, may be null. When null is used, validation objects will not be created. |