NXOpen.UF.Clone.CopyNmOpt Structure¶
NXOpen.UF.Clone.CopyNmOpt is an alias for NXOpen.UF.CloneCopyNmOpt_Struct
-
class
NXOpen.UF.
CloneCopyNmOpt_Struct
¶ Bases:
object
Refer to UF_CLONE_copy_nm_opt_s for documentation.
Fields
NXOpen.UF.CloneCopyNmOpt_Struct.NonmasterType |
when structure is being returned a string containing the name of a nonmaster type defined in the database, such as “specification” |
NXOpen.UF.CloneCopyNmOpt_Struct.Copy |
when structure is being returned a logical indicating whether this nonmaster type should be copied during a clone operation, imported, or exported. TRUE means that nonmasters of that type will be copied |