NXOpen.UF.Clear.SetObjList¶
-
Clear.
SetObjList
()¶ Refer to UF_CLEAR_set_obj_list for documentation.
Deprecated since version NX9.0: Please use following Assemblies::ClearanceAnalysisBuilder’s properties instead: ClearanceBetween() TotalCollectionCount CollectionOne(Two)Range CollectionOne(Two)Objects
Signature:
SetObjList(dataset, whichList, listType, listSize, tagArray)
Parameters: - dataset (Tag) – The dataset tag.
- whichList (int) – Is this for list 1 or list 2? Acceptable values are 1 and 2.
- listType (int) – The new type of list (UF_CLEAR_ALL_OBJECTS, UF_CLEAR_ALL_VISIBLE_OBJECTS, UF_CLEAR_ALL_BUT, UF_CLEAR_FIXED_LIST, or UF_CLEAR_LIST2_NOT_USED).
- listSize (int) – The size of tag_array.
- tagArray (list of Tag) – list_size The object tags (solids or facets) to be applied to the list.
License requirements: ASSEMBLIES MODULE