NXOpen.UF.Clear.SetInterfText¶
-
Clear.
SetInterfText
()¶ Refer to UF_CLEAR_set_interf_text for documentation.
Deprecated since version NX9.0: Please use Assemblies::ClearanceSet::SetInterferenceText() instead.
Signature:
SetInterfText(dataset, object1, object2, text)
Parameters: - dataset (Tag) – The dataset tag
- object1 (Tag) – The first object (solid or facet) in the pair
- object2 (Tag) – The second object (solid or facet) in the pair
- text (str) – The text to associate with the interference. The length of the text cannot be greater than the value assigned to the string constant MAX_LINE_SIZE.
License requirements: ASSEMBLIES MODULE