NXOpen.UF.Clear.IsPairIncluded¶
-
Clear.
IsPairIncluded
()¶ Refer to UF_CLEAR_is_pair_included for documentation.
Deprecated since version NX9.0: Please use Assemblies::ClearanceAnalysisBuilder::GetIsPairIncluded() instead.
Signature:
IsPairIncluded(dataset, object1, object2)
Parameters: Returns: A Tuple
Return type: A tuple consisting of (includeIt,reason,text)
includeIt(bool): Should this pair be included in the analysis?
reason(int): The reason the pair is included or excluded (one of UF_CLEAR_EXCL_NO_REASON, UF_CLEAR_EXCL_USER_DEF, UF_CLEAR_EXCL_SAME_COMP, UF_CLEAR_EXCL_SAME_PART, UF_CLEAR_EXCL_SAME_GROUP, or UF_CLEAR_EXCL_MATED_COMP).
text(str): The text associated with UF_CLEAR_set_pair_inclusion and UF_CLEAR_set_pair_exclusion when reason is UF_CLEAR_EXCL_USER_DEF, or an empty string is returned. Use UF_free((void *) *text) to deallocate memory when done.
License requirements: None