NXOpen.UF.Clear.AskObjectClearZone¶
-
Clear.
AskObjectClearZone
()¶ Refer to UF_CLEAR_ask_object_clear_zone for documentation.
Deprecated since version NX9.0: Please use Assemblies::ClearanceAnalysisBuilder::GetObjectClearanceZone() instead.
Signature:
AskObjectClearZone(dataset, objectArg)
Parameters: Returns: A Tuple
Return type: A tuple consisting of (clrZone,source)
clrZone(Tag): The clearance zone expression.
source(int): The source of the clearance zone (one of UF_CLEAR_USING_DEFINED_CZ, or UF_CLEAR_USING_DEFAULT_CZ).
License requirements: None