NXOpen.UF.Clear.AskObjAllButList¶
-
Clear.
AskObjAllButList
()¶ Refer to UF_CLEAR_ask_obj_all_but_list for documentation.
Deprecated since version NX9.0: Please use following Assemblies::ClearanceAnalysisBuilder’s properties instead: ClearanceBetween TotalCollectionCount CollectionOne(Two)Range CollectionOne(Two)Objects
Signature:
AskObjAllButList(dataset, whichList)
Parameters: - dataset (Tag) – The dataset tag
- whichList (int) – Determines which list to use: 1 = List 1 2 = List 2
Returns: A Tuple
Return type: A tuple consisting of (listSize,tagArray)
listSize(int): The number of objects in the list
tagArray(list of Tag): The array of objects (solid or facet) on the list. This should be freed by calling UF_free.
License requirements: None