NXOpen.UF.CgmSize_Struct.Mode¶
-
CgmSize_Struct.
Mode
¶ Structure UF_CGM_size_t specifies the size of geometry recorded in the CGM file. The size field of the UF_CGM_export_options_t structure is a structure of type UF_CGM_size_t. If the mode field of the UF_CGM_size_t structure is set to UF_CGM_SIZE_BY_SCALE, then geometry is sized according to the scale factor specified by the scale field. If the mode field is set to UF_CGM_SIZE_BY_DIMENSIONS, then geometry is sized to fit the dimensions specified by the dimensions field.