NXOpen.UF.Cgm.ExportOptions Structure¶
NXOpen.UF.Cgm.ExportOptions is an alias for NXOpen.UF.CgmExportOptions_Struct
-
class
NXOpen.UF.
CgmExportOptions_Struct
¶ Bases:
object
Refer to UF_CGM_export_options_s for documentation.
Fields
NXOpen.UF.CgmExportOptions_Struct.Colors |
Specifies how colors are applied to exported geometry. |
NXOpen.UF.CgmExportOptions_Struct.Widths |
Specifies how lines widths are applied to exported geometry. |
NXOpen.UF.CgmExportOptions_Struct.VdcMode |
Specifies how coordinates are represented in the CGM file. |
NXOpen.UF.CgmExportOptions_Struct.Size |
Specifies the size or scale of exported geometry. |
NXOpen.UF.CgmExportOptions_Struct.TextMode |
Specifies how text geometry is represented in the CGM file. |
NXOpen.UF.CgmExportOptions_Struct.Fonts |
Specifies how fonts are recorded in the CGM file. |
NXOpen.UF.CgmExportOptions_Struct.Reason |
Specifies the reason the CGM file is being exported. |
NXOpen.UF.CgmExportOptions_Struct.Tolerance |
A unitless value that controls the accuracy or smoothness of exported curve geometry. |