NXOpen.UF.Cgm.Color Structure¶
NXOpen.UF.Cgm.Color is an alias for NXOpen.UF.CgmColor_Struct
-
class
NXOpen.UF.
CgmColor_Struct
¶ Bases:
object
Refer to UF_CGM_color_s for documentation.
Fields
NXOpen.UF.CgmColor_Struct.ClrIndex |
Color index in the range [ 0 to UF_OBJ_MAX_COLOR ] |
NXOpen.UF.CgmColor_Struct.ClrName |
Color name, specified as a NULL-terminated ASCII string |
NXOpen.UF.CgmColor_Struct.ClrVals |
An RGB definition of the color, consisting of red, green, and blue values in the range [ 0.0 to 1.0 ]. |
NXOpen.UF.CgmColor_Struct.FavoriteIndex |
If the color is a favorite color, an favorite index in the range [ 1 to 30 ]. |