NXOpen.UF.Cgm.ExportCgm¶
-
Cgm.
ExportCgm
()¶ Refer to UF_CGM_export_cgm for documentation.
Signature:
ExportCgm(drawingSheet, exportOptions, fileName)
Parameters: - drawingSheet (Tag) – The tag of the drawingsheet to export. If set to NULL_TAG, the current display image is exported instead.
- exportOptions (
NXOpen.UF.Cgm.ExportOptions
Refer to UF_CGM_export_options_s for documentation.) – Specifies export options.If NULL, current session export options are used instead. If non-NULL, call UF_CGM_ask_default_export_options or UF_CGM_ask_session_export_options to initialize the structure before setting structure fields. Current session export options are not modified by structure values. - fileName (str) – The CGM filename
License requirements: None