NXOpen.UF.Cfi.SpawnCheckStatus¶
-
Cfi.
SpawnCheckStatus
()¶ Refer to UF_CFI_spawn_check_status for documentation.
Signature:
SpawnCheckStatus(processId)
Parameters: processId (int) – The process id returned by UF_CFI_spawn for the command that was run. Note that this is only returned for processes that are run concurrently. Returns: A Tuple Return type: A tuple consisting of (stillRunning,returnStatus) stillRunning(bool): If TRUE, the command is still running. If FALSE, the command has completed.
returnStatus(int): If still_running is FALSE, then this is the return status from the child process. If still_running is TRUE, then this will be set to zero. A return_status of 127 is set when the spawned command could not be found.
License requirements: None