NXOpen.UF.Cfi.Spawn¶
-
Cfi.
Spawn
()¶ Refer to UF_CFI_spawn for documentation.
Signature:
Spawn(program, numArgs, arguments, isConcur)
Parameters: - program (str) – The command to be executed. This command must either be a full path name, or the program must be found on the path.
- numArgs (int) – The number of arguments in the next array. These arguments will be passed to the command.
- arguments (list of str) – An array of character pointers for the arguments to be passed to the program. You may pass in a NULL if there are not any arguments. These arguments will be added in the order they are stored, so the command will be: program argument[0] argument[1] ... Switches must be formatted by the caller. On NT, switches take the form “-switch:value”, where on Unix switches take the form “-switch=value”.
- isConcur (bool) – If TRUE, the command will be run at the same time as the NX Open program, if FALSE, then UF_CFI_spawn will wait for the completion of the command prior to returning to the caller.
Returns: The process ID of the spawned process. This process ID can be used to check the status of the spawned process using UF_CFI_spawn_check_status.
Return type: int
License requirements: None