NXOpen.UF.Bound.AllData Structure¶
NXOpen.UF.Bound.AllData is an alias for NXOpen.UF.BoundAllData_Struct
-
class
NXOpen.UF.
BoundAllData_Struct
¶ Bases:
object
Refer to UF_BOUND_all_data_s for documentation.
Fields
NXOpen.UF.BoundAllData_Struct.NumMembers |
number of boundary members |
NXOpen.UF.BoundAllData_Struct.OpenClosedFlag |
flag to indicate if the boundary is open or closed UF_BOUND_OPEN or UF_BOUND_CLOSED |
NXOpen.UF.BoundAllData_Struct.PlaneMatrix |
tag of matrix of plane |
NXOpen.UF.BoundAllData_Struct.MinimumDistance |
distance from model space origin to plane |
NXOpen.UF.BoundAllData_Struct.MaxminBox |
maximum and minimum box of the boundary |
NXOpen.UF.BoundAllData_Struct.Tolerance |
boundary tolerances tolerance[0]: The maximum allowed tolerance that the boundary may deviate from the defining curves into the part tolerance[1]: The maximum allowed tolerance that the boundary may deviate from the defining curves away from the part. |
NXOpen.UF.BoundAllData_Struct.MembersData |
data of boundary members |