NXOpen.UF.Attr.GetUserAttributeLockWithTitleAndType¶
-
Attr.
GetUserAttributeLockWithTitleAndType
()¶ Refer to UF_ATTR_get_user_attribute_lock_with_title_and_type for documentation.
Signature:
GetUserAttributeLockWithTitleAndType(objectArg, title, type, index)
Parameters: - objectArg (Tag) – The object holding the attribute
- title (str) – The attribute title
- type (int) – The attribute type Valid values: UF_ATTR_integer UF_ATTR_real UF_ATTR_time UF_ATTR_null UF_ATTR_string UF_ATTR_bool UF_ATTR_any NOTE: If UF_ATTR_any is used, the first attribute encountered that matches the given title (and index), is returned
- index (int) – The array index (set to UF_ATTR_NOT_ARRAY if not an array)
Returns: A Tuple
Return type: A tuple consisting of (isLocked,hasAttribute)
isLocked(bool): The lock status of the attribute. Valid only if the attribute is set.
hasAttribute(bool): A set attribute has been found
License requirements: None