NXOpen.UF.Assem.UpgradeStatus Structure¶
NXOpen.UF.Assem.UpgradeStatus is an alias for NXOpen.UF.AssemUpgradeStatus_Struct
-
class
NXOpen.UF.
AssemUpgradeStatus_Struct
¶ Bases:
object
Refer to UF_ASSEM_upgrade_status_s for documentation.
Fields
NXOpen.UF.AssemUpgradeStatus_Struct.Failed |
true if any components could not be upgraded |
NXOpen.UF.AssemUpgradeStatus_Struct.NComponents |
length of the following two arrays |
NXOpen.UF.AssemUpgradeStatus_Struct.ComponentNames |
array of component names that failed to upgrade. This array must be freed using UF_free_string_array. |
NXOpen.UF.AssemUpgradeStatus_Struct.Statuses |
associated statuses with each file name. This array must be freed using UF_free. |