NXOpen.UF.AssemOptions_Struct.LoadWaveParents¶
-
AssemOptions_Struct.
LoadWaveParents
¶ Load Unloaded Wave Parents option. This field is only used if load_wave_data is set to UF_ASSEM_load_wave_data. When it is, this value controls the way in which parents of wave geometry are loaded: UF_ASSEM_none - Don’t load unloaded parents, but ensure partially loaded parents are fully loaded. UF_ASSEM_immediate - Load immediate parents of any WAVE data. UF_ASSEM_all - Load parents of WAVE data, and their parents, until no parents can be found. A parent part is one which contains geometry that is linked to another part. If part A has a LINKED_BODY which references geometry in part B, then set the load options as follows: load_wave_data = UF_ASSEM_load_wave_data load_wave_parents = UF_ASSEM_immediate If you load part A, then part B is loaded.